Close

Data Center Challenges: Top 3 Design Considerations

Prior to the pandemic, data center demands were relatively predictable. Not anymore.

With the remote worker locations constantly shifting and the further proliferation of connected devices, network management has become a major challenge. And it’s not just about provisioning enough routers and switches to keep the data flowing. Ensuring uptime, reliability, and security is far more complex in this highly-distributed environment.

Read More →
data center solutions

‘Connection-First’ Design Crucial for Today’s Complex Data Centers

Taking a step back to look at data centers holistically, and not just from the standpoint of the ‘tech’ involved, is vital to understanding how and why connectivity is essential. The big picture perspective also spotlights the need for connectivity to play into the design considerations from the point of data center design inception. With the expectations for reliable, consistent delivery of rapid speed and high performance for the largest hyperscalers in the world, it’s more critical than ever to explore the role connectivity plays as the road by which all connections are made and power travels.

Read More →

Reliability Testing: The Key to Ensuring Data Center Accuracy and Performance

Developments in cloud computing, the Internet of Things, and the proliferation of mobile devices in everyday technology have all made innovative, highly efficient data centers more necessary than ever. Ensuring that today's increasingly complex data centers are agile, adaptable, distributed, efficient and intelligent is a challenge for the ages. However, to achieve and maintain the highest levels of accuracy and performance in these almost futuristic structures running at high temperatures and high speeds, it is essential to carefully consider the often underappreciated but critical world of testing.

Read More →

Vivek Shah, Director, New Product Development, oversees the development of high-speed products in Copper Solutions Business Unit at Molex. He has over 12 years of experience in designing and developing high-speed products such as backplane connectors, IO connectors, and cable assemblies. His expertise includes Signal Integrity, Mechanical Engineering and Product Marketing. While at Molex, Vivek has successfully launched products from 25Gbps to 112Gbps data rates.