As 5G availability spreads and makes smart technology more widely available, edge computing servers will become commonplace.
We interviewed 207 qualified participants responsible for 5G in R&D, engineering, and product roles at network carriers. Their answers were eye-opening.
Almost half (46%) of carriers surveyed finished 2020 behind their plans. COVID-19 was a big culprit, with 54% advising the pandemic delayed their 5G deployment efforts. The good news? The pandemic is anticipated to have less of an effect (39%) on their future roadmap.
But they may not be what you expect…
Spectrum issues are most often cited as challenges — and by the widest margin. Lack of consumer/end-customer use cases and regulation impediments based on geography are numbers two and three. High capital requirements (28%) is fourth, but also the number #1 thing that has to change for carriers to meet 5G business goals.
When asked which 5G application would be the first to generate significant new business revenue, consumer devices led the way (43%). IIoT (35%) and fixed wireless access (33%) came next. Curious what came last on the list? Medical devices (19%).
Designing 5G capabilities into a device not only involves selecting the most appropriate 5G components, but also requires proficiency in properly incorporating sensitive RF antennas. Molex is unique in that it offers expertise in both areas. For carriers that are re-designing their networks, converting switches, or upgrading and deploying new cell sites, Molex can help you stay ahead of the 5G curve.
As 5G availability spreads and makes smart technology more widely available, edge computing servers will become commonplace.
Get relevant insights on what's driving the 5G expansion in the podcast.
How manufacturers can successfully position themselves for what comes next.
Learn more about the performance needs versus cost for these markets in the podcast.
With carriers facing growing data traffic demands, a transformation is required to power the next-generation networks to enable 5G and deliver increased bandwidth at low latency.
Companies involved in making 5G components require state-of-the-art testing to measure capabilities of beamforming, radiation emissions, high-gain antennas, low-loss and high-frequency connectors, and more.
The 5G rollout will transform and facilitate the adoption of emerging technologies in categories from healthcare to industrial and automotive.
How the new mobile standard makes the vision of connected driving become a reality.