Introducing the Hermetically Sealed Circular MT Assemblies

Did you know that Molex is more than a power connector manufacturing company?

Molex is a technology leader not only in copper interconnects, but also in Fiber Optics. Molex’s Fiber Optics division has a diverse product offering from industry standard connectors & panel adapters, standard and hybrid cable assemblies and backplane connectors to EMI containment adapters, active optical cables, optical flexplanes and the a
ctual
pulling of specialty fiber. We have been involved in designing and  manufacturing leading edge fiber optic interconnects & cable assemblies since 1988.

We have a diverse capability within our organization that you can take advantage of including – in-house design, testing, manufacturing and value-add assembly. A good example of this capability and ability to drive technology is why I am here today, to talk  to you  about our new addition to our ruggedized product line: The Hermetically Sealed Circular MT assemblies.

Traditionally hermetically sealed fiber optic connectors have been offered only with low fiber counts and in large space consuming connector shells. This new product
offers

  • A small footprint connector body  which fits into an area of 30mm
  • With up to 24 sealed fibers in this connector
  • AND is Hermetically sealed to 1×10 -6  millibars  of vacuum
  • This product is ideal for critical cannot fail applications in very harsh environments such as Oil & Gas exploration instruments & sensors, as well as military radar array systems.
  • We can provide these in a number of configurations to suit your requirements with either mulitmode or singlemode fiber.

Hermetic-mated-baseline

For more information on this exciting new Molex product, go to Molex.com and pull up the fiber optic section and look under the Ruggedized Solutions tab.